Understanding Project Directory Paths

If you are using iFIX Project Configuration with Remote Desktop Services, make sure that the Base and Language Paths are the same for each project. The locations of the project paths can differ, depending upon the user type. However, the Base and Language Paths should be the same for each project.

For instance, if you leave the Base and Language set to the defaults, the Base is set to C:\Program Files (x86)\GE\iFIX and the Language is set to C:\Program Files (x86)\GE\iFIX\NLS for each project.