Zoom Method Example
The following example zooms in on the Chart with a high and low vertical value of 50 and 10 and a high and low horizontal value of 75 and 35 for Chart1.
Chart1.Zoom 50, 10, 75, 35
Zoom Method ExampleThe following example zooms in on the Chart with a high and low vertical value of 50 and 10 and a high and low horizontal value of 75 and 35 for Chart1. Chart1.Zoom 50, 10, 75, 35
|
Check out the new features in the latest version of iFIX. See our free trials to add value to iFIX & Proficy.
|
![]() |