RuntimeVisible Property

Whether or not the document is visible in the Run-time environment.

Syntax

object.RuntimeVisible [= Boolean]

Properties

The RuntimeVisible property syntax has these parts:

Part

Description

object

An object expression that evaluates to an object in the Applies To list.

Boolean

Whether the document is visible.

Settings

The settings for Boolean are:

Value

Description

True

The document is visible in the Run-time environment. (Default)

False

The document is not visible in the Run-time environment.

Remarks

To display a picture that was opened with the RuntimeVisible property set to False, you must set the active window's Active property to True.

The following is an example of code that will set the RuntimeVisible and Active properties:

Dim doc As Object

Set doc = Application.Documents.Open("C:\Program Files (x86)\GE\iFIX\PIC\SAMPLE.GRF")

doc.ActiveWindow.Active = True

 

Applies To