CombinationKey Property

Indicates how the Control and Shift keys are used in defining the key combination for a key macro object.

Syntax

object.CombinationKey [= Value]

Properties

The CombinationKey property syntax has these parts:

Part

Description

object

An object expression that evaluates to an object in the Applies To list.

Value

0 - ComboKeyNone Neither the Control or Shift key is used in combination with the key code.

1-  ComboKeyCtrl Only the Control key is used in combination with the key code.

2 - ComboKeyShift Only the Shift key is used in combination with the key code.

3 - ComboKeyCtrlShift Both the Control and the Shift key are used in combination with the key code.

 

Applies To