Acknowledges new alarms for the specified block.
Syntax
AcknowledgeAnAlarm[DataPoint],
[intErrorMode],
[BsendMsg]
Properties
The AcknowledgeAnAlarm subroutine syntax has these parts:
Part
|
Description
|
DataPoint
|
String. (Optional) The name of the database block
for which you want to acknowledge alarms. If no block is specified, alarms
for the database block associated with the selected object are acknowledged.
|
intErrorMode
|
Integer. (Optional). The error mode.
0 (default) – Allows the subroutines to provide the
error messages. Errors are displayed in the form of a message box. If
no entry is made for the intErrorMode parameter, the default is used.
1 – Allows the user to handle the error messages.
Errors in the subroutines are passed back to the calling routine for handling.
2 – Writes errors to all destinations. No error messages
display. Instead, the errors are written to all iFIX destinations, including
the Alarm History window destinations using SendOperatorMessage.
|
BsendMsg
|
Boolean. (Optional). If TRUE, the message "value changed byxxx" will be sent to the alarm destinations. If FALSE, the message will be suppressed. |
Example