If a network problem occurs during startup, one of the error codes or
messages listed in the following table may appear.
Startup Error Messages
Error Code
|
Error Message
|
Description
|
1613
|
Duplicate name in local name table.
|
iFIX did not shut down properly prior to starting
back up. Restart the computer and iFIX.
|
1622
|
Name in use on remote node.
|
The node name assigned to the node is currently in
use on another node. Rename one of the nodes to correct this conflict.
|
8501
8502
|
Underlying network subsystem not ready.
TCPTASK: Failed to initialize network subsystem.
|
TCP/IP is not installed properly or is missing. Use
PING or TCPTASK to verify that the underlying TCP/IP is set up before
attempting to run iFIX.
|
8503
|
Windows Sockets API version mismatch.
|
When attempting to initialize the Winsock TCP/IP interface,
TCPTASK detected that the Winsock version is less than 1.1.
|
See Also