You can select an object by clicking it with the mouse. Objects can be selected in the picture itself or in the system tree. The selected object remains selected until you click another object. When you select an object, the object's handles appear, permitting you to change the object's size. For more information on object handles, refer to the Using Basic Drawing Tools section.
Selecting Multiple Objects
You can select multiple objects by enclosing two or more objects in a rectangle selector, or by selecting the first object and then control-clicking additional objects. The following figure shows both methods.