Flipping Objects

One simple way to change the way your objects appear in relation to each other is to flip them. When you flip an object, the object reflects along its vertical or horizontal axis and reappears as a mirror image of the original.

There are two ways to flip an object. You can flip an object simply by dragging a handle of an object from one side to its opposite side. The drawback to this approach is that it also stretches the object. The following figure shows a manually-flipped object that was accidentally reshaped.

Flipping Objects Manually

A more effective way to flip an object is to use the Flip Horizontal and Flip Vertical method. This method flips the object while maintaining its original size and shape. The following figure illustrates this effect.

Flipping Objects Effectively

How Do I...