Restoring the Alarm Summary Object's Default Settings

To restore the Alarm Summary object's default settings:

  1. In the iFIX WorkSpace, double-click the Alarm Summary object. The Alarm Summary Configuration dialog box appears.
  2. Click Reset. The default settings get applied to the selected Alarm Summary object.

TIP: Only the settings in the selected Alarm Summary object get restored. If you want other Alarm Summary objects that you create after this one to also use the same default settings, click Save. This saves your Alarm Summary settings to the AlarmSummary.ini file in the LOCAL folder (by default: C:\Program Files (x86)\GE\iFIX\LOCAL), so that subsequent Alarm Summary objects will apply these default settings when you first drop the object into your picture.

See Also