Editing a Query

After you create a query, it remains the current query until you change it. Using this feature, you can append a new query to the existing one and re-query the database. For example, suppose you create the following query:

{Type} ="AI" AND {Alarm Area 1} ="Boston"

This query displays all the Analog Input blocks in the Boston alarm area. By appending the query:

AND {AI LOLO Alarm}<= "10"

you can display only those Analog Input blocks in the alarm area which have a LOLO alarm value less than or equal to ten.

To locate blank cells in the database:

  1. In Classic view, on the View menu, click Properties.

-Or-

In Ribbon view, on the View tab, in the Settings group, click Properties.

  1. Select the Query tab and enter the following query.

{TAG NAME} = "*" AND {column_name}=""

    For example, to find blank cells in the Description column use the query:

{TAG NAME} = "*" AND {Description}=""

This query displays all the blocks in the database that have no text in their Description fields.

 

See Also

How Do I...