QPn Property

Specifies a string that equates to the current value assigned to the query property.

Syntax

object.QPn[= String]

Parameters

The QPn property syntax has these parts:

Part

Description

object

An object expression that evaluates to an object in the Applies To list.

String

The current value assigned to the query property. For example, the value assigned to QP1 could be Finance.

Remarks

These properties are designed to be variables for use in the SQL Select statement. When the query runs, it replaces the QPn placeholder with the string value.

See Also