CurrentRow Property

Identifies the number of the current row in the retrieved ADO record set.

Syntax

object.CurrentRow [= Long]

Parameters

The CurrentRow property syntax has these parts:

Part

Description

object

An object expression that evaluates to an object in the Applies To list.

Long

The zero-based number of the current record in the record array.

Remarks

The CurrentRow value is visible in the Data Control in Run mode. Use the MoveNext, MovePrevious, MoveFirst, and MoveLast methods to change the current row number.

See Also

Applies to