ADOCommand Property
Exposes the read-only Data Control's CommandTimeout value to allow users to configure a time-out duration in Visual Basic scripts.
Syntax
object.ADOCommand
Parameters
The object placeholder represents an object expression that evaluates to an object in the Applies To list.
Remarks
The data type of this property is ADODB.COMMAND.
If the value is not set, then Command object will use the default value of 30 seconds for the time-out.
Example
The following sample script demonstrates the use of the ADO CommandTimeOut:
' Create a ADODB.Command object
Dim objCommand As ADODB.Command
' Capture the current command instance into the newly create object
Set objCommand = vxData1.ADOCommand
' Set a new CommandTimeOut value in seconds
objCommand.CommandTimeout = 40
' Refresh the object
vxData1.RefreshData