MovePrevious Method Example
The following example is a script associated with a command button, that, when clicked, makes the previous row in the record set retrieved by the Data ObjectvxData1 the current row.
Private Sub CommandButton1_Click()
vxData1.MovePrevious
End Sub
NOTES (CIMPLICITY USERS ONLY):
- The name of the subroutine shown here follows standard VBA naming convention, which does not apply to CimEdit Basic script language.
- In CIMPLICITY, the following additional code must precede the first reference of vxData1 in its scope:
Dim vxData1 As Object
Set vxData1 = CimGetScreen.Object.Objects.Item("vxData1").OleObject