To create a query
that returns unique rows using the SQL Wizard:
- Run the SQL Wizard and on the Select Operation dialog box, click SQL Select.
- Proceed in the SQL Wizard until you reach the Select Columns dialog box.
NOTE: You can only return unique rows for your query in an SQL SELECT statement.
- In the Select Columns dialog box, select columns to include in your query.
- Select the Return Unique Rows check box.
- Click Next to continue creating the query.
- Or -
Click Back to return to the previous screen in the SQL Wizard.
- Or -
Click Finish if the query is done.
See Also