To animate a
query property with a Data link:
- In the iFIX WorkSpace, insert and configure a VisiconX Data Control.
- In the Create Row Filter dialog box, create a query that uses a query property.
- Insert a VisiconX Grid, ListBox, or ComboBox Control and animate it. Use the VisiconX Data Control as the animation data source.
- To insert a Data link object:
In Ribbon view, on the Insert tab, in the Objects/Links group, click Objects/Links and then Datalink.
- Or -
In Classic view, on the WorkSpace Insert menu, select Datalink.
- In the Datalink dialog box, select the source. This could be Caption for in-place entries. From the Data Entry list, select In-Place and if necessary, increase the Chars/Line value.
- Right-click the Data link to animate its caption. Select the Text tab.
- Click the Animate button for the Caption property. Select the Data link's caption as its data source and choose In-Place for Data Entry.
- Right-click the Data Control and animate the query property used in the Filter Options dialog box. Use the caption of the Data link as the animation data source.
- In the iFIX WorkSpace, switch to Run mode.
- Modify the caption in the Data link to change the rows displayed in the Grid Control.
See Also