Verifying and Editing an ODBC Data Source

Once you have configured the settings for an ODBC data source, you can verify that the information is correct and make changes at any time.

To verify information and edit the settings for an ODBC data source:

  1. Click the Start button and point to Programs, Administrative Tools, and then Data Sources (ODBC). You can also access the Administrative Tools folder from the Control Panel.

    The ODBC Data Source Administrator program opens.

  1. On the User DSN tab, select the appropriate data source from the list and click Configure. The ODBC Data Source Setup dialog box appears for the data source you selected.
  2. Check the settings and make any necessary changes.
  3. In the ODBC Data Source Setup dialog box, click OK.
  4. In the Data Source Administrator dialog box, click OK.

See Also

How Do I...