Installing the Oracle Driver

The steps that follow describe how to install the Oracle 10g Release 2 Client, so that you can use it with iFIX.

To install the Oracle driver:

  1. Run the setup program for the Oracle 10g Release 2 Client.
  2. On the Welcome screen, click Next.
  3. When prompted for an installation type, select Custom Installation and click Next.
  4. On the Destination screen, in the Name field, change the default setting by selecting the destination you used when installing the "Runtime" Client. The path should automatically change to the path associated with the name. Click Next.
  5. On the Available Product Components screen, select the Oracle Windows Interfaces 10.2.0.1.0 and click Next.
  6. On the Product-Specific Prerequisite Check screen, click Next.
  7. On the Summary screen, click Install. When the installation completes, a final screen appears.
  8. Click Exit to finish the install.

 

How Do I...