Time-Based Processing

Most applications work by acquiring and calculating data at regular intervals, defined in seconds, minutes, or hours. iFIX can perform any combination of time-based processing. This allows you to balance system resources between data that needs to be acquired quickly and data that can be acquired over longer intervals.

SAC can perform time-based processing in:

  • Subseconds (0.05 seconds to 0.95 seconds)
  • Seconds
  • Minutes
  • Hours

The frequency with which SAC retrieves data is called the scan time. For more information on scan times, refer to the Building a SCADA System manual.

See Also