Reports

Detailed reports are important tools for reviewing the performance of a process. They allow you to quickly grasp the relationships between specific pieces of manufacturing process data so that you can make effective decisions. Using any third-party reporting application that supports ODBC queries, you can create customized reports based on iFIX real-time and historical data. When you use iFIX real-time data, you generate the report with current data extracted from the iFIX database. When you create a report using iFIX historical data, you generate the report based on data gathered over a period of time.

For example, suppose you are the production manager of a cookie factory. At the end of each shift you want to generate a customized report that shows the amount of down time on each production line. You would use the Scheduler to request this report at certain times using iFIX historical data. In addition, if a failure occurs on a particular line you want to have your system automatically generate a report showing the tank level of each ingredient, the state of the mixer and dropper, and the temperature of the oven at the time of the failure. When a failure occurs, the requested iFIX real-time data is extracted from the iFIX database and displayed in a report. The data in this report can then be analyzed to help prevent future failures.

See Also