Nodes in iFIX

There are several types of nodes available using iFIX.

Types of Nodes

Type

Description

Local and Remote

When working with a distributed iFIX system, local refers to the node on which you are currently working and remote refers to any node that you need a communication link to access.

Stand Alone

When working with a centralized iFIX SCADA system, stand alone refers to a node that performs all functions. Stand alone nodes do not use a network.

SCADA Server

A SCADA Server (or SCADA node) runs the data acquisition and management component of iFIX. Usually, a SCADA node resides on the plant floor and has direct connections to the process hardware.

Blind SCADA Server

A blind SCADA Server (or blind SCADA node) uses no graphics display. This configuration frees up more of a computer's resources for data acquisition and network management functions. Graphics can be viewed using an iClient.

Run-time

A run-time node does not let you modify graphic displays or the process database. Pre-configured files are installed on these nodes so that you can monitor the process, change process settings, and acknowledge alarms.

iClient

An iClient (or view node) is the most common type of node. View nodes display the real-time graphics that come with iFIX. The term view node means that the node runs the graphics display program, but the node can run other applications, as well.

iClient Read Only

The iClient Read Only has the same functionality as an iClient, except that you cannot write to the iFIX database or to OPC servers. You also cannot construct SQL Insert or Update commands in an iClient Read Only node. You can, however, write to a relational database. The iClient Read Only is similar in functionality to PlantTV® for FIX, with the added benefit of leveraging the iClient features, such as the event scheduler, VBA, and ActiveX controls.