To set shape
preferences:
- In Classic view, from the iFIX WorkSpace menu, select User Preferences.
-Or-
In Ribbon view, on the Home tab, in the WorkSpace group, click Settings, and then click User Preferences.
- Click the Shape Preferences tab.
- In the Color area, click each button and select the shape's fade, foreground, background, and edge colors.
- In the Font area, select the default font, size, and style for text objects.
- From the Edge Style and Fill Style lists select the default shape edge and fill styles, respectively.
- In the Edge Width field, enter the default edge thickness, in pixels.
- From the Background Style list, select the default background style.
- In the Hit Test Size field, enter the minimum distance, in pixels required to select an object. When the cursor is within the specified distance, iFIX selects the object.
- From the Fade Type list, choose the default fade type.
- In the Blend field, enter how much of the fade color, in a percentage, will be mixed with the foreground color.
- In the Thickness field, enter the default thickness for pipe objects. You can enter any value from 10 to 300.
- From the Elbow Style list, choose the default elbow style for pipe objects.
- From the Start Cap and End Cap lists, choose the default start and end caps for pipe objects.
- Select the Remove Leading and Trailing Spaces check box to indicate that iFIX should remove extra spaces when Data Links are displayed in the run-time environment.