To create a toolbar:
- In Classic view, in the iFIX WorkSpace, from the WorkSpace menu, select Toolbars.
-Or-
In Ribbon view, on the Home tab, in the WorkSpace group, click Settings, and then click Toolbars.
- Click Customize.
- Click the Toolbars tab.
- Click Add Toolbar.
- Enter a name for the toolbar.
- Select the toolbar's owner from the Owner list. If the owner you want does not appear:
- Close the Customize Toolbars dialog box.
- Open a document of the associated type. For example, open a picture to select Picture as an owner.
- Repeat steps 1 through 6.
- Add buttons to the toolbar.
- Edit each button's script as needed.