To setup DCOM
support in the WorkSpace:
- If necessary, install the driver:
- Insert the I/O Drivers and OPC Servers CD into your CD-ROM drive. The CD spins up and the Driver CD splash screen appears.
- Click the Install Driver button.
- Select the driver name from the menu. For example for the MBE driver, select MBE - Modbus Eithernet v7.x.
- Click the Install Now button.
- Run the Data Server Installer. You can launch this application from the Start menu by pointing to Programs, iFIX, Tools, and then Data Server Installer. The Data Server Installer dialog box appears.
- Click Add to add an OPC server. The Add Server dialog box appears.
- Enter an OPC data source name in the Data Server field. For example, for the MBE driver, you might enter MBESOURCE in this field.
- Select the OPC server from the drop-down list in the OPC Server field. For example, for the MBE driver you would select Intellution.MBEOPC.
- In the Machine Name field, enter the local or remote computer name where the OPC Server resides.
- Click OK to save your changes.
- Configure the server from the iFIX program group. For example, for the MBE driver, select the MBE PowerTool option.
See Also