Button Properties Dialog Box

The Button Properties dialog box displays the following items:

Bitmaps List Box

Displays a list of bitmaps in the iFIX Local path.  You can select one of these bitmaps for the button or you can select a custom bitmap of your own by browsing to it.  If you select a custom bitmap, the image can be no more than 20 x 20 pixels and use no more than 16 colors.  

Preview

Displays a preview of the bitmap highlighted in the Current Directory bitmap list.

Category

Specifies the current category.  

Name

Specifies the name of the button you are configuring.  You can edit this name by entering the text you want.  

Description

Lets you enter a text description for the button you are configuring.  This text appears on the Buttons tab when you select the button.  

Screentip

Lets you enter a text description of up to 128 characters for the button you are configuring.  This text pops up when you place the cursor over the button.  

Edit Script

Lets you open the Visual Basic Editor, and enter or edit the current button's script.  

How Do I...