Applying Enhanced Chart Properties

There are several ways you can apply selected properties to your charts using the Chart Customization dialog box:

  • Select a new data set in the Data Sources list.
  • Click OK.
  • Click Apply.
  • Select the Apply to All Data Sources check box.

Each of these methods are described in the following table.

Methods of Applying Properties 

Use this method...

To...

Select a new data source in the Data Source list

Automatically apply properties based on the selected data source. This method takes precedence over other methods of applying properties: you do not have to click OK or Apply to apply the data source property, and, if you click Cancel after you have selected a data source, the properties are still applied.

Click OK

Quickly apply selected properties to your chart and close the Chart Customization dialog box.

No matter which method you use to apply properties, you must click OK to close the dialog box.

Click Apply

View a property change immediately without closing the Chart Customization dialog box. For example, if you want to change the color of a chart, change the color and click Apply. The color of the chart will change while the Chart Configuration dialog box stays on your screen.

You are not required to click Apply to apply properties to your chart.

Select the Apply to All Data Sources check box

Apply properties to all data sources added to a chart. Refer to the Applying Properties to All Data Sources section below for more information.

NOTE: The Apply to All Data Sources check box applies only during the current configuration session. The default (that is, the check box is cleared) is restored the next time you open the Chart Configuration dialog box.

Applying Properties to all Data Sources

iFIX allows you to easily define time, X and Y axis, grid, and legend properties for every data source you add to your chart. You can do this by simply selecting the Apply to All Data Sources check box on the Time tab on the Data Sources tab. For example, you may want all of the data sources in your chart to have the same legend. To accomplish this, click the Legend tab and select the properties you want. Next, select the Apply to All Data Sources check box. Exit the dialog box by clicking OK.