Click the following links for detailed process information:
- Stop the I/O driver manually from Mission Control
- Stop the I/O Driver from the Power Tool
- Stop the I/O driver from the iFIX Process Database
NOTE: If the OPC Client driver is added to the SCU, and you do not stop it, it will be stopped automatically when iFIX is shut down.
To stop
the I/O driver manually from Mission Control:
- Start Mission Control.
- Click the I/O Control tab. This tab displays a list of the drivers installed on your computer, along with the driver’s status (ACTIVE or STOPPED).
- From the Drivers list box, select the driver you want to stop.
- Click Stop.
To stop
the I/O driver from the OPC Client Power Tool:
From the Display Mode menu, choose Stop.
To stop
the driver from iFIX Process Database
- From the Drivers menu, choose OPC.
- When the Power Tool opens, choose Stop from the Display Mode menu.