To set your I/O Driver Power
Tool to connect automatically to the I/O Server on either a local or remote
machine:
- From Windows Explorer, open your iFIX folder, typically C:\Program Files (x86)\Proficy\iFIX, and select OPCDIDW.EXE.
- Create a shortcut by right-clicking the mouse and selecting Create Shortcut from the menu displayed.
- Right-click the new shortcut and choose Properties.
- Select the Shortcut tab.
- In the Target box, append one of the following command line parameters after OPCDIDW.EXE, as shown in the following examples:
Connection Type |
Command Line Parameters |
Example |
Remote |
/N remote_machine_name |
OPCDIDW.EXE /N Jake |
Remote |
/N remote_ip_address |
OPCDIDW.EXE /N 199.103.251.114 |
Local |
/L |
OPCDIDW.EXE /L |
This setup suppresses the I/O Driver Server Connection dialog box on Power Tool start-up. This is a good practice if you plan to always use the same server on the same computer.
See Also