When you access a topic in the OPC Client online help, it may not provide all the information you need. To learn more about a topic, you can:
- Use help links.
- Click the See Also button and select another topic.
Using Help Links
Blue words or phrases are links. Clicking a link either displays another topic or a pop-up window on top of the current topic. If you are using the keyboard, press Tab to move to the next link in the topic and press Enter to activate the link.
Links to other topics are blue with a solid underline and are called jumps. Jumps take you out of the current topic to a new topic. Links that display pop-up windows are blue italics with a solid underline. Pop-up windows display over the current window and are usually definitions of terms.
Using the See Also List
Most topics have a See Also button located directly under the topic title. Click the See Also button to display a list of topics related to the current topic. If you select one of the topics from the list, that topic displays. To get back to your original topic, click the Back button on the button bar.