Data Monitor Dialog Box

Starting Address

Displays the data received for the selected item in the format selected in the Format setting.

Quality

Displays the quality of the data in the selected item.

If the data quality is bad, the links in your operator displays show question marks by default. To save the last good value, enable the Latch data option. For more information about data quality, refer to Understanding Data Quality.

Format

Specifies the format or data type to use when displaying an item’s data. Possible formats include:

Format/Data Type

Displays

Byte

Unsigned 8-bit values

Char

Signed 8-bit values

Hex

8-bit hexadecimal values

Short

Signed 16-bit integers

Word

Unsigned 16-bit integers

Float

32-bit floating-point values (IEEE)

Long

Signed 32-bit integers

DWord

Unsigned 32-bit integers

Octal

Octal (unsigned integer) data

ASCII

ASCII text

Digital

Binary values

DblFloat

64-bit floating point values (IEEE)

Last Time Read

Displays the last time and date the I/O driver successfully read data from the process hardware for the selected item.

Last Time Written

Displays the last time and date the driver successfully wrote data to the process hardware for the selected item.

Time of Last Error

Displays the last date and time the driver failed to access the selected item in the process hardware.

Refresh

Click to refresh the data display with updated data from the driver.

See Also