To troubleshoot scripts that are
not firing properly in a schedule:
- In the run-time environment, click the Fire Now button for the entry that is not working properly. This button executes the script independently from when then script is scheduled to fire. Ensure that the script fires and runs properly.
- Check the entry's configuration by returning to the configuration environment and double-clicking the entry number to display the Modify Event Entry or Modify Timer Entry dialog box. Ensure that the parameters are set correctly.
- Check the SCU and ensure that SAC is running. Refer to the Setting Up the Environment e-book.
- Check the Database Manager and ensure that the block is on scan. Refer to the Building a SCADA Systeme-book.
- Use the Visual Basic Editor to debug the script.