Starting FixBackgroundServer as a Windows Service
To start FixBackgroundServer as a
Windows Service:
- Shut down iFIX.
- Ensure that you are logged in as an Administrator.
- On the Start menu, point to Programs, iFIX, and then System Configuration. The System Configuration Utility (SCU) window appears.
- From the Configure menu, click Local Startup. The SCU's Local Startup Definition dialog box appears.
- Select the "Run iFIX as a Service" check box, and click OK. This configures iFIX to run as a service.
- Click the Task Configuration button on the SCU toolbox. The SCU's Task Configuration dialog box appears.
- In the Filename field, enter the path and file name of the FixBackgroundServer application. By default:
C:\Program Files (x86)\Proficy\iFIX\FIXBACKGROUNDSERVER.EXE
- Select the Background Option button.
- Click Add to add FixBackgroundServer to the Configured Tasks list.
- Click OK.
- On the File menu, click Save to save the SCU file.
- Exit the SCU.
- Restart iFIX.