To modify an existing entry:
- Open the schedule that contains the entry you want to modify by double-clicking it in the Schedules folder of the iFIX WorkSpace system tree.
- Double-click the row number of the entry to display the Modify Timer Entry or Modify Event Entry dialog box.
- Modify the fields in the Schedule, Trigger, and Action areas as desired. For help on individual fields, click the What's This? (question mark) help button and select the field for which you want more information.
- Click OK. To save your changes, click the Save button on the Standard Toolbar.
TIP: You can also select an individual cell in the schedule's spreadsheet and change its value directly rather than accessing the Modify Timer Entry or Modify Event Entry dialog boxes. Your modifications are automatically put into effect when you exit the cell.