Creating One Shot Time-Based Entries

To create a one shot time-based entry:

  1. Open the schedule that you want to add the one shot time-based entry to by double-clicking it in the Schedules folder of the iFIX WorkSpace system tree, or create a new schedule by clicking the New Schedule button on the Standard Toolbar.
  2. Right-click a row in the schedule. From the pop-up menu, select Add New Timer Entry. The Add Timer Entry dialog box appears.
  3. Select the One Shot option button and enter the date and time at which you want the entry to occur.
  4. Enter the necessary information in the Schedule and Action areas. For help on individual fields within the Add Timer Entry dialog box, click the What's This? (question mark) help button and select the field for which you want more information.
  5. Click OK. To save your changes, click the Save button on the Standard Toolbar.

 

See Also