Creating Monthly Time-Based Entries

To create a monthly time-based entry:

  1. Open the schedule that you want to add the monthly time-based entry to by double-clicking it in the Schedules folder of the iFIX WorkSpace system tree, or create a new schedule by clicking the New Schedule button on the Standard Toolbar.
  2. Right-click a row in the schedule. From the pop-up menu, select Add New Timer Entry. The Add Timer Entry dialog box appears.
  3. Select the Monthly option button.
  4. Select the buttons for all of the days of the month that you want the entry to trigger. Select the End of Month check box to have iFIX automatically trigger the entry on the last day of the month.
  5. In the Start Time field, enter the time that you want the event to trigger.
  6. Optionally, select the Enable End Time/Interval check box to configure the entry to trigger repeatedly at a specific rate and for a specific duration of time. Enter the time that you want to stop the entry from firing in the End Time field. Enter the duration of time between occurrences of the entry in the Interval field.
  7. Enter the necessary information in the Schedule and Action areas. For help on individual fields within the Add Timer Entry dialog box, click the What's This? (question mark) help button and select the field for which you want more information.
  8. Click OK. To save your changes, click the Save button on the Standard Toolbar.

 

See Also