To select the
directories and folders to use in the Application Validator:
- In the iFIX WorkSpace, double-click Application Validator in the system tree. The Application Validator opens.
- On the File menu, click Select Directories. The Select Directories dialog box appears.
- Select the directories and folders for which you want to create baseline files.
You can select up to 500 directories and folders. Selecting a top level folder also selects all the folders included beneath this folder. Likewise, the same is true for deselecting folders. You can select any number of folders, as long as you don't exceed the 500 limit.
NOTE: The Application Validator does not handle directories named with characters outside of the ASCII character set.
Later, you can compare the changes in these folders since you last created this baseline.
- Click OK.