Running the Application Validator

You can run the Application Validator from the iFIX WorkSpace, the Windows Explorer, or the command line. Refer to the following table for more information.

Running the Application Validator

If you want to start the Application Validator from the...

Do this...

iFIX WorkSpace

Double-click the Application Validator icon in the system tree.

Windows Explorer

Double-click the AppValidator.exe file in the folder where you installed iFIX.

Command Line

From the DOS prompt type the AppValidator command with the desired command line options.

Refer to the Command Line Options for the Application Validator section for a full description of these options.