Button Script Sample Code
The following example shows code for a button object called MyExpert that gets the timer or event object, the event trigger name, and picture name, if any, from the Add Event dialog box. It passes this information in to the form using the GetCurrentObjectValues procedure, and then displays the form.
Private Sub MyExpert_Click()
Dim CurrentObj As Object
Dim EventName As String
'Set procedure object, event name, and file name
Set CurrentObj = MyExpert.ProcedureObject
EventName = MyExpert.EventProcedure
MyExpert.Property1 = frmOpenPicture.TextBox1.Value
'Pass the object and event name into the form
Call frmOpenPicture.GetCurrentObjectValues(CurrentObj,_
EventName)
frmOpenPicture.Show
frmOpenPicture.Hide
End Sub