XYHitTest Method

Returns information for a Pen based on the specified coordinates. Typically used with the MouseUp and MouseDown events.

Syntax

object.XYHitTest lfX, lfY, pDt, pfV, pszPenName, ppPen, lPenNum, pbReal

Properties

The XYHitTest method syntax has these parts:

Part

Description

object

An object expression that evaluates to an object in the Applies To list.

x

Double. The X coordinate where the mouse is clicked.

y

Double. The Y coordinate where the mouse is clicked.

pDt

Date. Returns the date for the Pen that corresponds to the specified X and Y coordinates.

pfV

Double. Returns the value for the Pen that corresponds to the specified X and Y coordinates.

pszPenName

String. Returns the name of the Pen that corresponds to the specified X and Y coordinates.

ppPen

Object. Returns the Pen object that corresponds to the specified X and Y coordinates.

lPenNum

Long. Returns the index in the Pens collection for the Pen that corresponds to the specified X and Y coordinates.

pbReal

Boolean. Returns True if the hit test was on a real point and False if it was on an interpolated point.

Remarks

This method is useful for performing operations based on Pen selection, or for creating data annotations. It returns the time and date of the clicked point, the value on the line, the pen's data source, a pointer to the Pen, the pen number, and whether the user clicked on a real or interpolated data point.

 

Example

Applies To