TimerEnabled Property

Specifies the run-time operation of the Timer object.

Syntax

object.TimerEnabled [= Boolean]

Properties

The TimerEnabled property syntax has these parts:

Part

Description

object

An object expression that evaluates to an object in the Applies To list.

Boolean

The run-time operation of the Timer object.

Settings

The settings for Boolean are:

Value

Description

True

If set in the Configuration environment, the Timer is started when the WorkSpace is switched to the Run-time environment. If set from False in the Run-time environment, nothing will happen, the user must call StartTimer.

False

If set in the Configuration environment, the Timer will not be started when the WorkSpace is switched to the Run-time environment. If set in the Run-time environment, the timer will be stopped.

 

Applies To