Timeout Property

Specifies the maximum amount of time the Chart may be paused (see Pause) before it will automatically resume (see Resume).

Syntax

object.Timeout [= Long]

Properties

The Timeout property syntax has these parts:

Part

Description

object

An object expression that evaluates to an object in the Applies To list.

Long

The maximum amount of time.

Remarks

If the Timeout property is set to zero (0), the chart will pause and not update until the Resume method is called.

 

Applies To