ShowGaps Property
Specifies whether the Pen ,GeneralDataSet, or RealTimeSPCDataSet should show gaps in the line indicating errors in the data sets.
Syntax
object.ShowGaps [= Boolean]
Properties
The ShowGaps property syntax has these parts:
Part |
Description |
object |
An object expression that evaluates to an object in the Applies To list. |
Boolean |
Whether to display gaps in the line. |
Settings
The settings for Boolean are:
Value |
Description |
True |
Data error gaps are displayed. |
False |
Data error gaps are not displayed. |
Remarks
Every data point has a value, timestamp, and a quality. If the quality code indicates a bad data sample, for example, device off line or communication access error, this code indicates that the sampling process could not get a valid reading at this point in time. With this field enabled, the Pen's data line will show a gap in the data line that indicates that there is no valid data.