SetGlobalHistoricalUpdateRate Method

Sets the historical update rate for the historical data sources in run mode.

Syntax

object.SetGlobalHistoricalUpdateRate hrs, mins, secs

Properties

The SetGlobalHistoricalUpdateRate method syntax has these parts:

Part

Description

object

An object expression that evaluates to an object in the Applies To list.

hrs

Long. The number of hours at which to set the duration.

mins

Long. The number of minutes at which to set the duration.

secs

Long. The number of seconds at which to set the duration.

Applies To