Sets the time for the Time Cursor position. The time of the Time Cursor is specified relative to a Pen, since pens can have different times on the same Chart.
Syntax
object.SetTimeCursorTime dt, lPenNum
Properties
The SetTimeCursorTime method syntax has these parts:
Part |
Description |
object |
An object expression that evaluates to an object in the Applies To list. |
dt |
Date. The time at which to set the Time Cursor. |
lPenNum |
Long. The index of the pen in the pen array for which you want to set the Time Cursor. |
Remarks
The time of the Time Cursor is specified relative to a Pen, since pens can have different times on the same Chart.