SetStatusFont Method

Sets the font for alarms with the specified status.

Syntax

object.SetStatusFont nStatusID, lpszFaceName, bStrikeout, bUnderline, bBold, bItalic

Properties

The SetStatusFont method syntax has these parts:

Part

Description

object

An object expression that evaluates to an object in the Applies To list.

nStatusID

Integer. The status of the alarm.
Valid values are:

0 – OK
1 – LOLO
2 – HIHI
3 – LO
4 – HI
5 – RATE
6 – COS
7 – CFN
8 – DEV
9 – FLT
10 – DSAB
11 – ERROR
12 – ANY
13 – NEW
14 – TIME
15 – IOF
16 – OCD
17 – UNDER
18 – OVER
19 – RANGE
20 – COMM
21 – DEVICE
22 – STATION
23 – ACCESS
24 – SQL LOGIN
25 – CMD
26 – DAT MATCH
27 – FLD READ
28 – FLD WRITE
29 – NO DATA
30 – NO XDATA

lpszFaceName

String. The font name to be displayed.

bStrikeout

Boolean. Specifies the Strikeout option for the text. If True, the text appears with a line through it.

bUnderline

String. The name of the event.

bBold

Boolean. Specifies whether the text is bold or not.

bItalic

Boolean. Specifies whether the text is italic or not.

Remarks

SetStatusFont is a Configuration environment method only.

 

Example

Applies To