SetManual Subroutine
Sets the specified block to manual mode.
Syntax
SetManual[DataPoint], [intErrorMode], [bSendMsg]
Properties
The SetManual subroutine syntax has these parts:
Part |
Description |
DataPoint |
String. (Optional) The name of the database block that you want to set to manual mode. If no block is specified, the database block associated with the selected object is set to manual mode. |
intErrorMode |
Integer. (Optional). The error mode. 1 – Allows the user to handle the error messages. Errors in the subroutines are passed back to the calling routine for handling. 2 – Writes errors to all destinations. No error messages display. Instead, the errors are written to all iFIX destinations, including the Alarm History window destinations using SendOperatorMessage. |
bSendMsg | Boolean. (Optional). If TRUE, the message "value changed byxxx" will be sent to the alarm destinations. If FALSE, the message will be suppressed. |