Specifies whether a Bitmap object's secondary image at the current index is being displayed as the primary (or mouse-up) image.
Syntax
object.SecondaryImageDisplayed [= Boolean]
Properties
The SecondaryImageDisplayed property syntax has this part:
Part |
Description |
object |
An object expression that evaluates to an object in the Applies To list. |
Settings
The settings for Boolean are:
Value |
Description |
True |
Display the secondary image. |
False |
Do not display the secondary image. |
Remarks
If SecondaryImageDisplayed is True, the primary image is displayed when the mouse is down. In all other cases the primary image is displayed. If a secondary image is not loaded, the primary image is displayed when the mouse is down.