ReplaceInString Method Example
The following example finds each occurrence of the string AI1 with the string FIX32.NODE1.AI1.F_CV by calling FindInString and then uses the lFirst, lCount parameter return values to replace AI1 with AI2, returning the new string in the sReplacement parameter. The operation is specified to include scripts in the search.
Dim lFirst As Long
Dim lCount As Long
Dim sMatchString As String
Dim bFound As Boolean
Dim bsuccess As Boolean
Dim sTarget As String
Dim sReplacement As String
sTarget = "FIX32.NODE1.AI1.F_CV"
FindReplace.FindInString "FIX32.NODE1.AI1.F_CV", 1, "AI1", 8, sMatchString, lFirst, lCount, bFound
FindReplace.ReplaceInString sTarget, "AI2", sMatchString, lFirst, lCount, 8, sReplacement, bsuccess