Specifies whether to allow multiple entries of the same event in the event queue.
Syntax
object.QueueEvents [= Boolean]
Properties
The QueueEvents property syntax has these parts:
Part |
Description |
object |
An object expression that evaluates to an object in the Applies To list. |
Boolean |
Whether to allow multiple entries in the queue. |
Settings
The settings for Boolean are:
Value |
Description |
True |
Allow multiple entries in the queue. |
False |
Prevent multiple entries in the queue. |
Remarks
If a Timer event is configured to occur every 5 seconds and it takes longer than 5 seconds to execute the event, the event will not be placed in the queue if QueueEvents is set to False. If QueueEvents is True, the event handler will occur for each event fired once the first event is acknowledged.