PieType Property

Specifies the constraints of the angle included between the StartAngle and EndAngle properties.

Syntax

object.PieType [= Integer]

Properties

The PieType property syntax has these parts:

Part

Description

object

An object expression that evaluates to an object in the Applies To list.

Integer

The type of pie to display.

Settings

The settings for Integer are:

Value

Description

1

The included angle is <= 180. (The pie is a wedge). (Default)

2

The included angle is > 180. (The pie is a cut out).

3

There is no restriction on the included angle.

 

Applies To